How to use existing projects built w/CS+ for another device of the same family?
Last Updated:06/14/2017
Question:
How can I use an existing project that I built with CS+ as a CS+ project for a different device?
Answer:
To change devices, start a new project by going to the [Create Project] screen and check [Pass the file composition of an existing project to the new project]. Specify the existing project and create a new project for a new device.
This will allow you to keep the option settings, etc., of the existing project for the new project targeting a different device.
For details, see “2.6.2 Create a new project” in the User’s Manual: Start.
Note that you cannot construct a new project by only replacing the device file in an existing project.
Suitable Products
CS+ (formerly CubeSuite+) |