Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

How to add include files (CS+ Integrated Development Environment)

Last Updated:06/07/2017

Question:

I am using the CS+ integrated development environment.

I am trying to create a file that I want to let a source file include. Do I need to specify the option settings of the build tool?

Answer:

You need to set the include file path in the properties of the build tool.

When you register (*) a file with an extension to be recognized as an include file in a project, a path to the file is automatically set for the include file path in the properties of the build tool.

For details about how to add a file to a project, see this site.

* Registering in the project tree

Suitable Products
CS+ (formerly CubeSuite+)