Skip to main content
Renesas Singapore - Knowledgebase

File Created during Startup of CS+

Last Updated:11/22/2017


What is the file that is created during startup of CS+ and automatically generated at next startup even if deleted?


A file named "xxxx.mtud" is automatically created when CS+ starts.

Note: The "xxxx.mtud" file contains project configuration information such as the panel position and breakpoint position. If this file has been deleted, CS+ starts with the default setting and automatically creates a new file.

Suitable Products
CS+ (formerly CubeSuite+)
  • Was this article helpful?