Skip to main content
Renesas Singapore - Knowledgebase

Error message: CC-RX compiler V. 2 section AAA overlaps section BBB

Latest Updated:10/29/2014


When I use the CC-RX compiler V. 2, it produces the following error message. What should I do about it ?

E0562321: Section "section name AAA" overlaps section "section name BBB"


In [Property] of the CC-RX (build tool), review the setting of [Section start address] (-start option) in the [Link Options] tabbed page.
When the addresses were allocated by the linker, the area for section BBB had an overlap with the area of section AAA.
Change the addresses specified for the allocation of section AAA or section BBB.
Suitable Products
CS+ (formerly CubeSuite+)
C/C++ Compiler Package for RX Family