Skip to main content
Renesas Singapore - Knowledgebase

Why building operation did not stop even if I click execute Build in menu

Latest Updated:09/10/2007


[High-performance Embedded Workshop V.4, V.3]  Even though I clicked an execute Build from the Build menu,the building operation did not stop. Why?


Execute Build is canceled after executing the Build command for the current file(or executing the current phase) in High-performance Embedded Workshop.

Please choose [Build->Terminate Current Tool] If you don't recieve a reply after awhile from project builder, the current process may have crashed. A file which is output from a crashed tool is invalid.

Please re-execute the phase by deleting these output files.

Suitable Products
High-performance Embedded Workshop