Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

Are there differences between file generated using Debug and Release?

Latest Updated:09/10/2007

Question:

Are there any differences between the [mot] file generated using the [Debug] configuration and that generated using the [Release] configuration?

Answer:

There's no difference between them.
At default settings, when you build with the [Debug] configuration, the [*.mot] file is also generated.
So you don't have to re-build with the [Release] configuration only to generate the [*.mot] file.
Suitable Products
High-performance Embedded Workshop