Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

After installing emulator software how the can I view the build menu?

Latest Updated:12/26/2014

Question:

I have installed the emulator software but the build menu is not displayed in the High-performance Embedded Workshop. How can I get the build menu to be displayed?

Answer:

The following are reasons for no build menu display.

  1. Compiler package is not installed:
    → With the multi-install feature, in particular, the problem is often that the compiler is not installed in the active environment.

    When performing a multi-installation, it is necessary to install the compiler package in each environment. Please confirm that the compiler package is installed in your active High-performance Embedded Workshop environment.
    To confirm installation, refer to FAQ1000231.

    If the compiler package has not been installed, install it at this time. For instructions concerning the multi-install feature, refer to the following URL.
    http://www.renesas.com/products/tools/ide/install_manager/index.jsp
  2. Installed version of High-performance Embedded Workshop or compiler is older than the version used when creating the workspace:
    → When opening an existing workspace, always confirm the versions of the High-performance Embedded Workshop and compiler package.
    Refer here to confirm the toolchain version used in the High-performance Embedded Workshop.
Suitable Products
High-performance Embedded Workshop
C/C++ Compiler Package for SuperH Family
C/C++ Compiler Package for RX Family
C/C++ Compiler Package for M16C Series and R8C Family [M3T-NC30WA]
C Compiler Package for R32C Series
C Compiler Package for M32C Series [M3T-NC308WA]
C/C++ Compiler Package for H8SX, H8S, H8 Family
E1 [R0E000010KCE00]
E20 [R0E000200KCT00]
E10A-USB
E8a
E10T-USB
E8
E100
E200F
E6000H
E6000
PC7501