Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

Why can’t I write an Intel HEX format file with M3T-SRA74 to MCU?

Latest Updated:12/11/2006

Question:

I am using the Flash Development Toolkit, but I can’t write an Intel HEX format file I created with M3T-SRA74 to the MCU.

Answer:

The Flash Development Tool Kit does not support Intel HEX format files when writing to the MCU.
Convert your file to the Motorola S record format.
Refer to FAQ 106405 for details on how to convert your file to the Motorola S record format.
Use the HEXTOS2 bundled with M3T-SRA74 (V.4.10 Release 02 and later) for the conversion.
Suitable Products
Assembler Package for 740 Family [M3T-SRA74]
Flash Development Toolkit