Skip to main content
Renesas Singapore - Knowledgebase

Which device name I should select in [Device and kernel selection]?

Latest Updated:06/23/2011


[Flash Development Toolkit V.3, V.4]I cannot find the device name I wish to use in [Device and kernel selection] window when creating project. Which device name I should select?


Confirm that your Flash Development Toolkit supports the target device by referencing the Supported Device Table below. Select the device name as listed in the “Select Device” example in the [Device and kernel selection] window.

For Flash Development Toolkit V.4, click here.

For Flash Development Toolkit V.3, click here.
Suitable Products
Flash Development Toolkit