Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

What function to record the previous parameters of FDT Ver.3.0 and V.4?

Latest Updated:06/04/2004

Question:

[Flash Development Toolkit V.3, V.4] Is there a function to record the previous parameters of the FDT Ver.3.0 (HS6400FDIW3SR) and V.4(R0C00000FDW04R) ?

Answer:

Yes, there is.The latest four workspaces are automatically recorded when selecting "open a recent project workspace". This log cannot be erased.
Suitable Products
Flash Development Toolkit