Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

Rewriting and erasing data flash memory_RL78

Last Updated:09/20/2017

Question:

Does the Data Flash Library Type04 provide the specification of rewriting and erasing data flash memory of the RL78 family?
Does using library functions allow to read and write the data flash memory?

Answer:

For rewriting and erasing data flash memory of the RL78 family, refer to the user’s manual for Data Flash Library Type04.
Use the library functions for Data Flash Library Type04 so that you can read and write the data flash memory.
Suitable Products
RL78 Family
Data Flash Libraries