Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

What are S & SPS in Timing chart after acceptance of interrupt request?

Latest Updated:03/01/2005

Question:

(Interrupts)   In the figure "Timing chart after acceptance of interrupt request", what are "S" and "SPS"?
Also, what is the "waiting time for post-processing of pipeline"? [2005/03/01]

Answer:

"S" is the stack pointer.
"SPS" is the page selected by the stack page selection bit of the CPU mode register.
"Waiting time for post-processing of pipeline" is the internal CPU processing time for the preceding instruction. When instructions are executed continuously, this processing is executed simultaneously with the first two cycles of the next instruction so no wait time is generated. However, wait time is generated when an interrupt occurs.
Although the expression "pipeline" is used, there is no queue buffer, etc. in the 740 Family. (#104768)

Suitable Products
3803H
3803L
3823
3850A
3858
38D2
38D5
7544
7545
7546
7547
7548
7549