Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

Ports P00-P03 & P54-P57 set input mode; key-on wakeup for input to P00

Latest Updated:03/01/2005

Question:

(Interrupts)   Can ports P00 to P03 and P54 to P57 be set to input mode and key-on wakeup enabled only for input to P00? [2005/03/01]

Answer:

Yes.
Key-on wakeup can be enabled/disabled for individual pins in the key-input control register settings. (#104954)
Suitable Products
38D2