Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

Can a single-power operational amplifier be used as dual-power?

Latest Updated:10/01/2006

Question:

Can a single-power operational amplifier be used as a dual-power operational amplifier?

Answer:

Yes. Check the supply voltage range and in-phase input voltage range.

Suitable Products
Operational Amplifiers
USB2.0 Host Controller
UPD720102
UPD720101
UPD720100A