Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

What's the base metal of 3 terminal regulator when exposed to pin?

Latest Updated:12/01/2011

Question:

The base metal  of the 3-terminal regulator is exposed at the roots of a pin.

Answer:

There is no problem. If the lead is plated up to the thinner part, the product is good.
Suitable Products
3 Terminal Regulators