Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

What is resistance between input and output of UPD5200, 5201 and 5205?

Latest Updated:09/01/2007

Question:

For the UPD5200, 5201, and 5205, what is the resistance value between input and output when the switch is OFF?

Answer:

The resistance value is not specified when the switch is OFF.
In this case, a leakage current flows. Refer to the section for source (drain) off-leakage current in the electrical characteristics.
Suitable Products