Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

Is the absolute drain current max rating of 8 A the total for 2 elements?

Latest Updated:10/01/2007

Question:

The uPA2755A power MOSFET is a product with 2 elements, but is the absolute maximum rating of drain current of 8 A the total for the two elements?

Answer:

No. The absolute maximum rating of drain current of 8 A is the rating for just one element.
In the case of two elements, the absolute maximum rating of drain current is restricted by the total dissipation.
Suitable Products
Power MOSFETs