Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

Are there data's for temperature such as 0℃, -20℃, -55℃, or 100℃?

Latest Updated:09/02/2013

Question:

The 2SK1522 datasheet states that the gate to source cutoff voltages Vgs(off) is 2.0 V min and 3.0 V max. What is the temperature characteristic? Is there any data for when the temperature is 0℃, -20℃, -55℃, or 100℃?

Answer:

On the lower right of page 4 of the 2SK1522 datasheet, there is a graph that shows the temperature characteristics of VGS(off).
Suitable Products
Power MOSFETs for General Switching