Skip to main content
Renesas Singapore - Knowledgebase

What are -1 and -2 variations in UPC1093?

Latest Updated:12/01/2011


It seems that this product, UPC1093, has variations such as -1 and -2. What are they?


These are products with special specification that differ from general-purpose products with regard to Vref.
At present, Vref is as follows.
The contents of the special specification are subject to change. For details, refer to the shipping documents.

Vref (unit:V)
Suitable Products
CMOS comparators
bipolar comparators
Shunt Regulators