Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

Is the CTR rank of part No. PS2801C-4-F3 the same as the PS2801C-1?

Last Updated: 01/22/2018

Question:

Is the CTR rank of part No. PS2801C-4-F3 the same as the PS2801C-1?

Answer:

The CTR rank applies only to the PS2801C-1, and it does not apply to the PS2801C-4.
Refer to the following comments in the data sheet.
Suitable Products
Photocouplers / Optocouplers