Skip to main content
Renesas Singapore - Knowledgebase

What is a derating curve?

Latest Updated:12/01/2011


What is a derating curve?


Derating refers to thermal design in which the allowable power consumption is restricted according to the rise in the ambient temperature. A derating curve is a characteristics curve that indicates the total power dissipation (PT) vs. the ambient operating temperature (TA.)

When TA= +80°C in an 8-pin SOP (with PT = 440 mW and Rth (j - A) = 227°C/W @ TA = 25):

The characteristics for each package type are shown in the graphs below.

Remark If the diagonal lines of the derating curves are extended, the value at PT=0 is the maximum junction temperature (125°C in the case of operational amplifiers and comparators).

Suitable Products