Does the CL described in suggested operations apply to each channel?
Latest Updated:07/01/2006
Question:
For an operational amplifier, when a package has multiple channels (i.e., 4 or 2 channels), does the load capacitance (CL) described in the recommended operating conditions apply to each individual channel?
[Example: uPC842]
Recommended operating conditions
Answer:
Yes, this value applies per channel when using a package with more than one channel.
Suitable Products
Operational Amplifiers |
USB2.0 Host/Peripheral Controller |
UPD720150 |