Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

Does the CL described in suggested operations apply to each channel?

Latest Updated:07/01/2006

Question:

For an operational amplifier, when a package has multiple channels (i.e., 4 or 2 channels), does the load capacitance (CL) described in the recommended operating conditions apply to each individual channel?

[Example: uPC842]
Recommended operating conditions

Answer:

Yes, this value applies per channel when using a package with more than one channel.
Suitable Products
Operational Amplifiers
USB2.0 Host/Peripheral Controller
UPD720150