Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

Can I use a single power supply of +5 V using 4 V to 16 V?

Latest Updated:03/01/2006

Question:

The recommended power supply voltage for a low-noise wideband dual operational amplifier(uPC4570) is ±4 V to ±16 V. When using a single power supply, can I assume that this recommended value is 4 V to 16 V?
Can I use a single power supply of +5 V?

Answer:

The power supply voltage range for a single power supply is 8 V to 32 V. You therefore cannot use a single power supply of 5 V.
Suitable Products
Operational Amplifiers
USB2.0 Host/Peripheral Controller
UPD720150