Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

What is max rating of internal diode between drain and source of MOSFET?

Latest Updated:08/01/2005

Question:

What is the maximum rating of the internal diode between the drain and the source of a MOSFET?

Answer:

There is no rating for the internal diode by itself.
The forward current and withstand voltage are as listed in the absolute maximum ratings.
Suitable Products
Power MOSFETs