Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

What are the difference between TA = 25°C and TC = 25°C?

Latest Updated:07/01/2006

Question:

Two conditions are described for the total dissipation parameter in the power ratings of a power transistor or a power MOS FET: TA = 25°C and TC = 25°C. What is the difference between these conditions?

Answer:

The specification at TA = 25°C in the power ratings refers to the total power dissipation of a discrete semiconductor element in an environment with an ambient temperature of 25°C.
In this case, the thermal resistance from the heat source to the ambient air is expressed as Rth(j-a).

The specification at TC = 25°C in the power ratings refers to the total power dissipation when the semiconductor element (case) itself has been forcibly cooled, i.e., when temperature of the package surface is kept at 25°C.
Note that the ratings may include the note "with infinite heat sink". However, in actual use, it is very difficult to make the package surface temperature exactly 25°C, and if you also take derating into account, the allowable power will in fact be somewhere in between TA = 25°C and TC = 25°C.

Related FAQ items
Thermal Design

Suitable Products