Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

How is the series regulator used?

Latest Updated:12/01/2004

Question:

How is the series regulator used?

Answer:

The series regulator is connected in series with the load.
It detects fluctuation of the output current and input voltage by using an operational amplifier and holds the output voltage constant by controlling a variable resistor connected in series with the load.

Suitable Products
Power Management Linear
bipolar comparators