Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

What is Power Dissipation Derating (ΔPD/°C or ΔPC/°C)?

Latest Updated:02/01/2008

Question:

What is Power Dissipation Derating (ΔPD/°C or ΔPC/°C)?

Answer:

This is a rate of decrease in Power Dissipation (the light-emitting side PD and the light-receiving side PC) when the ambient temperature rises 1°C.

In the case of the PS2502, the following data is shown as Power Dissipation Derating (of the light-emitting side) in the maximum absolute ratings in the data sheet.



This power dissipation derating of the light-emitting side (ΔPD/°C) is shown as a linear inclination of at least 25°C on the data sheet (characteristic curve).



Power Dissipation Derating of the light-receiving side is also shown on the data sheet.
Suitable Products
Diodes for Constant Voltage
Photocouplers / Optocouplers