Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

What is GBP?

Latest Updated:12/01/2011

Question:

What is GBP?

Answer:

GBP stands for gain-bandwidth product, and is usually calculated at a frequency of 10 kHz. The GBP can be assumed to be within the Aυ vs. f characteristics range.



The shaded area indicates the range permitted when designing a device.
In this example, therefore, it is not possible to design a 60 dB amplifier with a frequency of 100 kHz.
Suitable Products
Operational Amplifiers
USB2.0 Host/Peripheral Controller
UPD720150