Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

TPS-1 Watchdog Error with Parallel Host Interface

Last Updated:06/01/2017

Question:

What happens if a watchdog error occurs when the TPS-1 is used with a parallel host interface? Does the TPS-1 configuration need to be downloaded again?

Answer:

The TPS-1 generates a diagnostic alarm for the controller and starts sending "0" (IOPS=BAD) until the TPS-1 gets a RESET. There is no need to download the configuration again.
Suitable Products
TPS-1
  • Was this article helpful?