TPS-1 Firmware Download via JTAG
Last Updated:06/01/2017
Question:
We would like to try downloading firmware onto the TPS-1 via the JTAG port. Does the existing TPS-1 firmware/hardware/software support this functionality?
Answer:
It is possible to download the the TPS Updater over the JTAG interface (production process).
Suitable Products
TPS-1 |