Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

TPS-1 Fast Startup Time

Last Updated:06/01/2017

Question:

How long does the TPS-1 need for "Fast-Startup"?

Answer:

Qualifying for the term "Fast-Startup" requires a start-up time of 500 ms or less. This period must be enough for a device to come to a full operating condition (to achieve this, for example, the data can be saved permanently in the device). The TPS-1 starts within this "Fast-Startup" period; start-up times down to 255 ms were achieved by evaluation.
Suitable Products
TPS-1
  • Was this article helpful?