Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

Minimum TPS-1 to Host MCU SPI Speed

Last Updated:06/01/2017

Question:

What is the slowest permissible SPI speed between the TPS-1 and a host MCU?

Answer:

The slowest SPI speed hasn’t been specified. However, using slow SPI speed may affect the performance of handling event and cyclic data.
Suitable Products
TPS-1
  • Was this article helpful?