Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

What are the optimization settings in e2 studio when running SSP?

Latest Updated:10/11/2016

Question:

What optimization settings are used by default when running e2 studio with SSP projects?

Answer:

In the most current SSP release (as of Oct 12, 2015) the default optimization setting in e2 studio for SSP build is -O2. This is different than the default setting for previous SSP builds, where the default setting was -O0 (None), and may impact  projects built on previous releases. If an issue results from this new optimization setting, please revert to no optimization.  You can do this by selecting project Properties, C/C++ Build, Settings, Optimization and then adjusting the Optimization level via the drop down menu at the top right. Click Apply.

Read the Release Notes for your specific release for more information on current Optimization settings.