Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

Troubleshooting TraceX installation

Last Updated: 05/03/2016

Overview

This FAQ details some troubleshooting information for installing correctly TraceX on your PC system.

Goal

Verifying that the correct installation settings were used.

Notice

On the Synergy gallery, there is a notice about the installation requirements for TraceX:

Solution

  1. Verify that you have administrative rights on the PC
  2. Execute the setup.exe as administrator, by right clicking on the setup.exe file and choose this option from the pop-up window as shown below:

Note: please do not confuse this with the .msi installer located in the same installation folder

What if the option "run as administrator" is not available?

Contact your PC system administrator to get the proper rights.

  • Was this article helpful?