Skip to main content
Renesas Singapore - Knowledgebase

sf_uart_comms Module Guide Resources

Last Updated:08/03/2017


Where can I find the references to module guide resources for the Module module on module?


Information on the module guide itself and the associated resources and known issues are available here.

Module Guide

The sf_uart_comms module guide is targeted for SSP 1.2.0 (and above) and the SK-S7G2 Kit.

The sf_uart_comms module guide describes what the module does, how to add it to your project, how to configure it, the associated APIs and provides an application project with a code walk through so you can quickly learn how to use the sf_uart_comms module in your own design. We recommend that you have the SSP ISDE open and inspect the module stack, configuration information and code while reading over the application project description.

The most recent versions of the sf_uart_comms module guide application note, application project and import guide are available here

Know issues

  • Refer to the most recent release notes for known issues, available here.

Associated Resources

  • None available currently
Suitable Products
SSP 1.2.0 and above
  • Was this article helpful?