Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

r_sci_i2c Module Guide Resources

Last Updated:11/27/2017

Question:

Where can I find the references to module guide resources for the I2C SCI HAL module on r_sci_i2c?

Answer:

Information on the module guide itself and the associated resources and known issues are available here.

Introduction

The I2C SCI HAL module is a high-level API for I2C Master Applications and is implemented on r_sci_i2c. The I2C SCI HAL module uses the SCI peripheral on the Synergy MCU. Callbacks are provided for transmit complete and receive complete.

The I2C SCI HAL module supports the following features:

  • Support for I2C SCI operations
  • Support transactions with a slave I2C device
  • Callback support

Module Guide

The I2C SCI HAL module guide is targeted for SSP 1.2.0 and above and the SK-S7G2 Kit.

The most recent versions of the I2C SCI HAL module guide application note, application project and import guide are available here.

Module Guide Resources

The following application projects are available from the Renesas web site at the referenced url.

  • PDC Web Camera Getting Started Guide - Application Project here.
  • HMI Brushless DC (BLDC) Motor Controller - Application Project here.
  • Getting Started with the Weather Panel Application- Application Project here.
  • The I2C SCI HAL module is used in the Developer Examples available as a template when a project is created in SSP for the DK-S7G2. You can find a Knowledge Base article that describes the Developer Examples and how to create a project using the template here.

Known issues

Refer to the SSP release notes for known issues, available here.

 

Suitable Products
SSP
  • Was this article helpful?