Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

r_sce Module Guide Resources

Last Updated:11/27/2017

Question:

Where can I find the references to module guide resources for the Module module on module?

Answer:

Information on the module guide itself and the associated resources and known issues are available here.

Introduction

The Secure Cryptographic Engine (SCE) HAL module is a high-level API for random number generation, digest computing (hash), data encryption and decryption, digital signing and verification. It is implemented on r_sce. The SCE is a dedicated hardware block that can perform cryptography related functions. The functionality provided by the SCE varies across the Synergy MCU Series.

The SCE HAL module configures the cryptographic module, which allows user to build cryptographic protocols for security with the following cryptographic primitives:

  • Random-number generation
  • Data encryption and decryption using AES or Triple DES (3DES) algorithms
  • Signature generation and verification using the RSA or DSA algorithms
  • Message-digest computation using HASH algorithms SHA1, SHA224, or SHA256
  • Key generation- AES wrapped keys, RSA plain text and wrapped keys

 

Module Guide

The SCE HAL module guide is targeted for SSP 1.2.0 and above and the SK-S7G2 Kit.

The most recent versions of the SCE HAL module guide application note, application project and import guide are available here.

Module Guide Resources

The following application projects are available from the Renesas web site at the referenced url.

  • Getting Started with Cryptography - Application Project here.

Known issues

  • Refer to the SSP release notes for known issues, available here.
Suitable Products
SSP
  • Was this article helpful?