Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

Where do I find additional resources to help me develop with the Synergy Platform?

Last Updated:01/08/2018

Question:

Where do I find additional resources to help me develop with the Synergy Platform?

Answer:

Published  material can be found at these locations:

Prof IoT Blogsclick here             Just click on the relevant tag on the right side of the page to select material on a particular topic.

Application Notesclick here     Select Documentation and check App Notes then click on Filter. Scroll through the list of Module Guides (documents that cover a specific SSP module and include a working application project as a hands-on exercise) and Application Notes (documents that cover a specific feature or capability of the Synergy Platform) to select the topics of most interest.

Videosclick here     Scroll through the right side tab to find topics of interest.

Knowledge Base Articlesclick here     Search for topics using to top of the page search bar. Use "Synergy" as a key word to focus on Synergy related content. 

Renesas Rulz Synergy Forum Postsclick here     Scan for topics or select the "More" pull down and then "Tags" to get a list of topics to filter for.

Renesas Academyclick here     After logging in, select Course Catalog, Renesas Synergy, and then Renesas Synergy Course. Scroll through the available modules to find the ones of interest.

Synergy Book:     click here     The Synergy Book covers the basics of the Renesas Synergy Platform from initial installation of the tools to creating a simple design. Select your area of interest by Chapter, Project or watch a Tutorial Video.

SSP User's Manual: click here    The SSP User's Manual provides background on the Synergy Software Package, and details on each module available to use in development. Useful as an introduction and as a detailed reference during design and debugging. The most up to date revision is available on the Synergy Gallery in the Synergy Software Package page in the Documentation Tab.

SSP Data Sheet: click here    The SSP Data Sheet has an inventory and overview of each of the components and layers included in SSP along with estimates for memory requirements and an indication of how each module was tested and verified. The most recent version, 1.2.0, can be found on the Synergy Gallery in the Release Archive tab. 

Synergy Platform MCU Hardware User's Manuals: click here    The Synergy Hardware Manuals provide details on the hardware resources used by associated SSP modules. These manuals can be helpful when there detailed are questions about the underlying hardware implementations. Details on the specific implementation of industry standards, for example, can typically be found in these manuals. From the Synergy MCU page, select the MCU of interest in the left side guide bar and then Documentation. Check the box in the Filter window for User's Manuals: Hardware and then click filter. The available documents will be listed.

Technical Updates: click here    Technical Updates are errata and other important updates that could impact your design. From the Synergy MCU page, select the MCU of interest in the left side guide bar and then Documentation. Check the box in the Filter window for Technical Updates and then click filter. The available documents will be listed.

 

Online Chat

For quick answers to Synergy Platform related questions that the above resources have not helped you with you can access the online chat system for the Synergy Platform. If the chat monitor is available, a chat Icon will be displayed on the right hand side of any Synergy page on Renesas.com or on the Synergy Gallery.

Chat Online    ChatOnline.PNG

 

Chat Offline    ChatOffline.PNG

 

Suitable Products
SSP