Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

What do I need to know to get the webserver demo to work with NetX Duo for 1.1.0-alpha.1?

Latest Updated:10/11/2016

Question:

What do I need to do to get the Synergy Webserver Demo working with NetX Duo for the SSP 1.1.0-alpha.1 release?

Answer:

In order to get the Webserver demo working you need to follow these simple guidelines:

1) Make the changes shown in the attached files.

demo_nx_http_application.c

demo_nx_http_httpserver_query.c

2) Deselect the nx and nx_http_server components from the configuration tab and select nxd and nxd_http_server in their place.