What can I do when I get the following error: Can't find a source file at "C:\ExpressLogic/ssp\src\framework\el\tx\tx_src\synergy\tx_thread_schedule.c"
Latest Updated:09/19/2016
Question:
What do I do to fix this error: Can't find a source file at "C:\ExpressLogic/ssp\src\framework\el\tx\tx_src\synergy\tx_thread_schedule.c"
Answer:
Click on the ThreadX source component in the configurator. This will compile the source and then the contents of this file will become visible.