Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

Is there an Example Project showing QSPI sub-sector Erase with FileX?

Latest Updated:10/04/2016

Question:

Is there an example project that shows a sub-sector erase of a QSPI memory using FileX?

Answer:

An example SK-S7G2 project for SSP 1.1.0 is attached. Note that Wear Leveling is not yet supported as of SSP 1.1.0.

https://renesas-rabbit.mindtouch.us/@api/deki/files/1792/S7_SK_QSPI_FILEX_SUBSECTOR_ERASE.zip

Suitable Products
SSP 1.1.0