Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

USBX Device Class CDC ACM Module Guide Resources

Last Updated:03/01/2018

Question:

Where can I find the resources for the USBX Device Class CDC ACM module guide?

Answer:

Information on the module guide itself and the associated resources and known issues are available here.

Introduction

The USBX™ Device Class CDC-ACM module is a high-level API for USBX Device Class CDC-ACM module applications and is implemented on the USBX Port CDC for USB Full Speed (USBFS) or USB High Speed (USBHS). The USBX Device CDC-ACM module uses the USB and data-transfer peripherals on the Synergy MCU. A user defined callback can be created to determine when the stack activates or deactivates the USB CDC-ACM class.

 

Module Guide

The USBX Device Class CDC ACM module guide is targeted for SSP 1.2.0 and above and the SK-S7G2 Kit.

The most recent versions of the USBX Device Class CDC ACM module guide application note, application project and import guide are available here.

Module Guide Resources

The following useful user manuals are included in the X-Ware documentation package available here.

  • USBX Host Stack User’s Manual
  • USBX Device Stack User’s Manual

The following useful module guides and application projects are available from the Renesas web site:

  • USBX Device Class HID Module Guide- Application Project here.
  • USBX Device Class Mass Storage Module Guide- Application Project here.
  • USBX Device Class CDC-ACM Module Guide- Application Project here.
  • USBX Host Class HUB Module Guide- Application Project here.
  • USBX Host Class CDC-ACM Module Guide- Application Project here.
  • USBX Host Class Mass Storage Module Guide- Application Project here.

You can find all USBX Synergy projects and documents by searching for "USBX Synergy" on Renesas.com here.

 

Known issues

  • Refer to the SSP release notes for known issues, available here.

 

Suitable Products
SSP
  • Was this article helpful?