Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

R_SCI_UART Module Guide Resources

Last Updated:04/18/2017

Question:

Where can I find the references to module guide resources for the UART HAL module on r_sci_uart?

Answer:

The UART HAL module guide is targeted for SSP 1.2.0 and the SK-S7G2 Kit.

The UART HAL module guide describes what the UART HAL module does, how to add it to your project, how to configure it, the associated APIs and provides an application project with a code walk through so you can quickly learn how to use the UART HAL module in your own design. We recommend that you have the SSP ISDE open and inspect the module stack, configuration information and code while reading over the application project description.

The most recent versions of the UART HAL module guide application note, application project and import guide will soon be available from the Synergy Gallery:  here

Know issues

  • No known issues as of posting date

Associated Resources

  • A USB to UART Pmod module is available from Digilent here:  here 
  • A Pmod module for an RS-232 interface is available from Digilent here: here 
UART on r_sci_uart module (SSP 1.2.0)
  • Was this article helpful?