Module Guide Wiki- r_adc
API Functions Operational Overview Selection Configuration Typical Application Application Example Resources Errata
Introduction
The ADC HAL module implements an API for analog-to-digital conversions and is implemented on r_adc. It supports the ADC12, ADC14 and ADC16 for the associated peripherals available on Synergy MCUs. A user-defined callback can be used to process the data each time a new sample is complete.
Features
- 16-Bit A/D Converter, 14-Bit A/D Converter and 12-Bit A/D Converter
- Multiple Operation Modes
- Single Scan
- Group Scan
- Continuous Scan
- Multiple Channels
- All analog channels available on MCU
- Up to 28 channels
- Temperature sensor channel
- Voltage sensor channel
- All analog channels available on MCU