Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

Im getting a build error about _sbrk having multiple definitions. How do I fix this?

Latest Updated:08/01/2005

Question:

The pictograph display segments are driven by the uPD16432B, but what is the method for accessing addresses of the RAM for pictograph display?

Answer:

Pictograph display refers to character display.
When reading 4.11 Commands in the uPD16432B Data Sheet, replace "character display RAM" with "pictograph display RAM".
In other words, in the mode setting, specify "001: Write to character display RAM," and set the addresses range to "00H to 07H."
Suitable Products
Synergy
  • Was this article helpful?