Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

How is temperature calibration done on Synergy MCUs TSN?

Latest Updated:12/19/2016

Question:

How do I calibrate the Temperature Sensor (TSN) so I can get the same readings from chip to chip?

Answer:

In the initial Synergy MCU silicon, WS2, the TSN readings are not calibrated, so you may find variations from chip to chip. In production devices the calibration registers will be set correctly.
Suitable Products
MCU WS2