Skip to main content
Knowledgebase
Home
Renesas Singapore - Knowledgebase

How do I use USB Drivers with Synergy Kits on Windows 10?

Last Updated:12/08/2017

Question:

How do I use the USB CDC drivers with Synergy kits on Windows 10?

Answer:

Windows 10 will automatically detect the USB CDC drivers that are used with Synergy Kits. The Class Code of the USB Device on the Synergy Kit should be verified to be set as Miscellaneous. See the below screen shots that illustrate this setting.

USBX Config.png

USBX Misc.png

 
SSP