Skip to main content
Renesas Singapore - Knowledgebase

How do I download new application projects for the Synergy platform?

Latest Updated:09/19/2016


I notice there are a few example designs (Project Templates) that come up in e2 studio after I have selected my target board. How do I add more of these application projects?


Project Templates come up when you add a Synergy Project within the ISDE as seen below:


You can access more Synergy Application Projects, by importing them instead. You will find these Application Projects on the Renesas web site on the Tools and Kits page:

Use the Documentation Tab, then check sample codes and then search to get a list of all the example designs. Simply import the Application Project as instructed in the associated Getting Started Guide downloaded with the project files.