Skip to main content
Renesas Singapore - Knowledgebase

How do I change the granularity on the ThreadX tick clock?

Latest Updated:09/19/2016


The default granularity on the ThreadX clock Tick is 10ms. Is there a way to change this?


The granularity of the Tick on ThreadX will be changeable via a CGC API call in a future SSP release. When the release date is available this post will be updated with that information. Once the API is available an example use will be show here.